Tag Archives: industrial networks

Smart Networks for the Future of Automation

From |

Written by Gareth Chamberlain

Throughout my life I have seen huge changes in the way IT has moved in the commercial sector. From multiple standalone servers taking up huge spaces and needing dedicated employees to look after the well-being of each one, to today where all the servers are combined in to a single physical piece with hosted virtualised servers on the physical platform.

I’m also lucky enough to be witnessing the same changing shift within the industrial sector. Engineers who have only been used to dealing with serial devices are now being asked to dive into the world of IT with Ethernet, Wireless and IT network protocols, with projects that demand real time data back to a central server.

smart_networks_topology

Continue reading →

Are you getting enough fibre in your life?

From |

Written by Mark Harries, Business Development Manager- I/O and Networks

Five top tips for fibre optic applications from Phoenix Contact

1.       Why choose fibre optic as a solution?

Fibre optic cables have the advantage of being able to transmit data over much longer ranges than copper cables. For example Ethernet cables are limited to a distance of 100m, whereas fibre cables can transmit data over distances of 45km.

Fibre Optic Graph

As the above diagram illustrates, fibre optic cables do not suffer with data rate loss in relation to the cable length. This makes no difference in a fibre optic application.

Continue reading →