Written by Deepan Patel, Industry Manager- Infrastructure
New features alert!
With Niagara 4.9 recently released, I have some new innovative features that are now available from our Infrastructure solutions to share with you. Don’t take these solutions only for Building Automation projects, we can do so much more with Niagara such as Email/SMS alerts, Data Logging, HTML5 autogenerated pages, visualisation engine, etc. Speak to me today and I can explain how!
- Our ILC 2050 controller now offers via its Shell environment, the ability to create IP Static Routes. For those networking experts this reduces the requirement of a Layer 3 switch. Now that’s a game changer!
2. Improved CPU load performance with the latest firmware release.
Continue reading

Consider the possibilities of having all the functionality of a building controller but with up to 63 I/O terminals directly connected to the controller, an integrated 4 port Ethernet switch, M-Bus and DALI modules, again directly connected to the controller, multi-protocol support and all
running on the Niagara 4 framework and it’s available in an industrial platform…what more could you want?