Tag Archives: Fibre Optic

The missing link

From |

Written by Gary Nelson- Senior Product Manager, Device Connections and Gareth Chamberlain- Product Manager, Cyber Security & IT Automation

In the world of smart networks, communication is key. But when do you make the decision of which connection technology to use?

Designing a network is always an intensive process, planning out what is needed and how devices will communicate with one another. Talking to people involved with each process, talking to the safety engineer and talking to the controls engineer and many other people. You have planned out the subnet and if any other network protocols are to run across the topology. But the one thing most network designers forget is what media and what connection is going to be used.

Continue reading

Are you getting enough fibre in your life?

From |

Written by Mark Harries, Business Development Manager- I/O and Networks

Five top tips for fibre optic applications from Phoenix Contact

1.       Why choose fibre optic as a solution?

Fibre optic cables have the advantage of being able to transmit data over much longer ranges than copper cables. For example Ethernet cables are limited to a distance of 100m, whereas fibre cables can transmit data over distances of 45km.

Fibre Optic Graph

As the above diagram illustrates, fibre optic cables do not suffer with data rate loss in relation to the cable length. This makes no difference in a fibre optic application.

Continue reading