Tag Archives: photovoltaic connector

Photovoltaic Plug Connector Featuring a Large Conductor Cross-Section

From |

The custom-assembly Sunclix plug connector (available up to 16 mm²) from Phoenix Contact makes it possible to contact conductor cross-sections from 6 mm² to 16 mm².

It was developed to answer the needs of ever-larger PV units in which the distance between module or string and the generator junction boxes or inverters is steadily increasing. Conductors with a large cross-section are required to minimize the transfer loss in the solar cable.

Continue reading →