Tag Archives: energy monitoring

A Glass of Beer

From |

Picture the following scenario. It’s a hot and sunny day and the weather is absolutely scorching. Just then, you are offered 2 glasses of beer – one foamy and one non foamy.

Which glass of beer would you choose?

beer3

Continue reading →

Remote Access to Energy Data

From |

Energy data collected using the Phoenix Contact EMpro family of measuring devices can now be monitored and analyzed remotely via a Web interface. This is made possible by two new Ethernet communication modules with an integrated Web server that allow measuring devices to be quickly and easily integrated into existing Ethernet networks.

Continue reading →