Author Archives: Steffi Lim

Steffi Lim

About Steffi Lim

Steffi is the MARCOM Manager with Phoenix Contact SEA.

Future Proofing Industry Seminar in Yangon, Myanmar

From |

Our slogan: “Inspiring Innovations”. It embodies what we do – Phoenix Contact never fails to come up with new and innovative products for the industry. As such, we are honored to be one of the market leaders and trendsetters of our industry.

Together with our partner in Myanmar, Synopsis Technology, we were proud to have brought you the “Future Proofing Industry” Seminar, held on the 31st of May 2018 at Lotte Hotel Yangon.

Seminar Poster

Alongside the topic of driving innovations, the main highlight of this “Future Proofing Industry” seminar was to introduce new applications and products for the education sector in Myanmar. It is of paramount importance to help the future engineers be ready for the industry.

Within the short time span of a day, we were elated that we had the opportunity to share our company history and actual success stories across South East Asia. Aside from that, we managed to introduce our innovative products as well.

First speaker: Mr Jiang

Our first speaker, Mr Jiang, who is also our Solution Manager, spoke about our new Industrial Cloud and Networking products for the first half of the seminar. Ideas and experiences were shared with the attendees.

Second speaker: Mr Maw Kon

The second speaker of the day was Mr Maw Kon, who is from Phoenix Contact Myanmar. He introduces our bread and butter products – the various connectors ranging from Terminal blocks to heavy duty connectors.

Third and final speaker: Mr Gary

Our last speaker, Mr Gary, never fails to draw the attentions of the attendees when it comes to introducing our surge protection devices. Live demonstrations and interactive activities were carried out and our attendees were all having a blast.

Last but not least, there was a mini competition held during the seminar.  All the attendees were encouraged to participate in the #futureproofingseminar and @phoenixcontactsea photoshoots. All they needed to do was to just take a photo during the seminar and upload them on their Facebook with the hashtag #futureproofingseminar together with a tag @phoenixcontactsea! The winner of the seminar was announced via our official Facebook page!

Make-before-break – Terminal Blocks for CT Test

From |

Make-Before-Break

Make-Before-Break (MBB) is a term “Denoting a switch or other device in which a new electrical connection is made before the existing one is broken”. In short, it simply means, shorting the circuit before disconnecting it.

You may know about MBB when purchasing a relay. But do you know there are terminal blocks designed with MBB in mind too? These MBB terminal blocks can usually be found in power industry applications.

For those who are familiar, you may have come across this term (MBB) during a Current Transformer (CT) testing on a protection relay. However, do you know the importance of ensuring MBB when conducting a CT test with your Terminal? Or what the consequences will be of not having a terminal blocks that comes with a MBB feature during the test?

Protection Relay

A CT will certainly be at risk of being destroyed or even worse (Explosion!) if the secondary is left open circuit while the primary current is present. This is due to the insulation failing from the “higher than rated” voltage that occurs. Therefore it is extremely important to ensure MBB before conducting a live testing. A good terminal block with MBB feature will definitely help you provide the extra mile in ensuring safety.

How does the MBB terminal blocks function and what does it look like?  Here are some good examples of a good MBB terminal block.

  1. A good MBB terminal block must have the feature where shorting is always present first before you are able to break the circuit. It would be best if the terminal blocks are able to automatically perform the short circuit for you whenever it is being disconnected during the CT test.
    Short Circuit function closed Short circuit function open
  2. Clear indication of Short Circuit and disconnection must be visible and this allows your engineers to have an ease of mind during testing.
    PTME
  3. Good MBB terminal blocks should have safe and easy to operate features. Having said that, these features can help to cut short the time while testing (shorten the risk) and ensuring the safety of the person that is conducting the CT test.
    PTME Terminal Blocks for CT Test

So where can you find good MBB terminal blocks for your applications? Phoenix Contact, of course!

With 94 years of experience manufacturing and designing terminal blocks for the Power Industry. Phoenix Contact has never stopped developing new innovative testing terminal blocks that will suits your application, at the same time ensuring safety and quality.

For more info, check out this video of our PTME terminal blocks or visit our website!

If you have more inquiries, feel free to contact us at marketing@phoenixcontact.com.sg and we will get back to you as soon as possible.

Copper Connections – Why Settle for Less?

From |

Have you ever wondered what your current screw terminal block is made of? Does it have copper connections or steel connections?

Rusting car

Similarly, have you ever wondered why a wire is made out of copper? I did a search and Google told me this.

“With its exceptional current carrying capacity, copper is more efficient than any other electrical conductor Because of its superior conductivity, annealed copper is the international standard to which all other electrical conductors are compared . … Another advantage is that copper oxide also conducts electricity.” (www.copper.org)

We know that copper is well-known for its good conductivity; that is why it is used in most electrical components. What about Terminal blocks? You will be surprised that most of the screw terminal blocks in the market are not made of copper. Not convinced? I dare you to take the magnet challenge

Continue reading

Introducing IIOT to your Clients – The PT Functional Terminal Blocks

From |

When you introduce IIOT to your client, one of the first questions your client will ask you is “What is IIOT?” (Yes, we get that a lot).

Confusion in IIOT

The typical look our clients are giving us when we talk about IIOT

Many manufacturers are baffled when they were asked to implement IIOT in their plant.

Well IIOT is not as complex. Here’s a sentence to explain what IIOT is:

“Using smart machines to consistently capture data in order to improve inefficiencies.”

See. It’s not that hard, is it?

When we further explain the sentence above, “smart machines” are simply referring to intelligent products like PLC or sensors that are able to help you in generating or gathering data.

Smart Machines

Smart Machines are getting smarter by the day

Smart machines allow data to be aggregated and analyzed in real time. With more accountability and control over equipment, workers can better predict maintenance issues and make faster decisions.

Not forgetting the ultimate motive “to save cost”.

Rain Money

Feel like a million bucks when you automated your business, and save half the installation cost. (Courtesy: Red Granite Pictures)

If you’re wondering how we can save you the effort and cost in installing IIOT systems, read on

The Revolutionary Test Plug Redux – FAME , FAME 2 and now FAME 3!

From |

Phoenix Contact's FAME 3

It was 2 years ago when I have first blogged about our revolutionary panel testing system – FAME systems that helped many of our customers worldwide in simplifying their protection relay panel testing procedure and at the same time ensuring the safety of the person who is conducting the test.

Do check out my previous blog “FAME 2- Enter, Push, Twist and Remove”, I did explain why Phoenix Contact FAME system is such a revolutionary testing system.  If you are dealing issues with your protection relay testing or any needs of installing a panel testing component, make sure you stay with us in this blog as I will review some updates and features that might be beneficial  to you.  No worries if you have missed out the previous blog, you can still read it here. Continue reading

Living in a Singapore HDB flat

From |

As a Malaysian, I grew up living in landed property houses; we are lucky in the sense where we have more land area for the individual to enjoy. Why do we love landed property so much? Well, you can easily associate the lifestyle of living in landed properties with building your control panel with single of double deck terminal blocks. Let me show you why. Continue reading

CLIPSAFE – Your one-stop junction box solution

From |

The “Blame Game”

Have you ever been bothered by such a situation?  Picture this, you have just completed your run on a beautiful day only to return home and realize that your feet are full of blisters. Should you put the blame on the shoe manufacture for using a material that is too tough, or would you blame the socks company for using a material that is too soft?

shoes

Things can potentially get uglier when it comes to planning for or executing a project. Have you had the unfortunate experience of opening a ‘Brand X’ junction box, to find yourself having ‘Brand A’ terminal blocks and maybe some ‘Brand C’ cable glands or markings inside. If there is a fault, who you should go to?

You may potentially find yourself being trapped in the “Blame Game” if you are having two or more different suppliers involved.  And if you have ever been trapped in one, you will know that the chances of successfully finding a solution and getting out is very minuscule.

What if there was a supplier who could provide you with a one-stop shopping experience?

CLIPSAFE – Your one-stop junction box solution

Over the years, many of our customers have requested Phoenix Contact to provide one-stop services where they not only purchase standalone components but are able to purchase a solution. We realized it made perfect sense for us to develop a portfolio of “basket or box” which would allow us to further improve our customers’ buying experience. This was the genesis of our CLIPSAFE range of junction boxes.

CLIPSAFE family of boxes

CLIPSAFE Family

 

As we all know, a junction box is just like the body. A healthy body needs a healthy heart – the components to be installed in the junction boxes. With more than 92 years of component manufacturing experience, you are assured we have maintained, and improved, on the quality of our ‘hearts’ over the past 9 decades.

Phoenix Contact’s CLIPSAFE junction boxes offer you the flexibility in choosing various hassle-free solutions.

Ex and NEMA 4X junction boxes equipped according to customer specifications

You can obtain CLIPSAFE enclosures fully equipped with terminal blocks and cable glands on request. Terminal boxes are delivered with the corresponding equipment approval in accordance with ATEX and IECEx for use in potentially explosive areas.

Steel CLIPSAFE box

CLIPSAFE Hi-grade Steel

 

Ex control boxes according to customer specifications

Individual control boxes with electronic components are available on request. With detailed engineering and planning, we will be able to support you in any complicated field-bus or control boxes requirements.

CLIPSAFE Control Box - Steel

CLIPSAFE Control Box – Steel

Empty Enclosure Ex or NEMA 4X

Still unable to make up your mind as to which components need to be installed in your junction boxes? Fret not.

You can always maintain the flexibility to design and assemble your own components as required by selecting our CLIPSAFE empty boxes.

Choose the right junction box housing for your application; from Stainless Steel to GRP material. We have more than 140 Ex-approved and NEMA 4X versions. Custom dimensions and surface treatments for Stainless Steel are available on request. The delivery is carried out with the corresponding components’ approval in accordance with ATEX and IECEx.

CLIPSAFE Empty Box - Steel

CLIPSAFE Empty Box – Steel

Empty Ex or NEMA 4X enclosure machined to customer specifications

Simply means junction boxes with pre-treated holes and cut outs. We adapt the housing to your request to include threads, drilled holes and rectangular cutouts while taking into account Ex-standards in accordance with ATEX and IECEx. The delivery is carried out with the corresponding components’ approval.

Empty box with flange plates and cover

Empty box with flange plates and cover

With all four types of CLIPSAFE offers, Phoenix Contact believes we will be able to address your needs. Not to forget, a good solution always comes with good quality and design. Do check out our CLIPSAFE Quality and Introduction videos below!

Long Awaited BT Terminals!

From |

Ladies and Gentlemen, Wait no further!

The long awaited Phoenix Contact BT terminal blocks are finally ready!

Allow me to present to you what we have to offer. Continue reading

Building installation with push-in three-level terminal blocks

From |

Thanks to the new PTI 4 three-level installation terminal blocks with push-in connection technology from Phoenix Contact, rigid conductors up to 6 mm² can be easily and directly wired without tools. The terminal blocks are specially tailored to the requirements of the electrical installation and the distributor construction, thanks to their compact design.

freistellen mit Pfad CD-Inlay einbauen Network Interfaces fg

The snap-in, no-screw disconnect slide with status indicator makes contacting the neutral busbar easy and safe. The function shaft on each level provides for easy potential distribution, thanks to the flexible jumper system. Each terminal point can be clearly marked and, in addition to the testing facility, has its own test connection in the function shaft.

Thanks to the insertion force, which has been reduced by 50 percent, it is possible to insert solid and stranded conductors with ferrules and cross sections from 0.5 to 6 mm² without tools. The built-in actuation lever allows fully insulated release with any tool. The orange-colored button indicates the actuating element. This prevents the terminal from being activated accidentally. Flexible conductors without ferrules can also be connected, from 0.2 mm by actuating the lever.

The push-in three-level terminal blocks share all the system characteristics with the CLIPLINE complete terminal block series and are therefore compatible with all installation terminal blocks from Phoenix Contact.

Modular marshalling patchboard concept with innovative color coding system

From |

The new push-in PTMC marshalling patchboards from Phoenix Contact achieve up to 20 percent higher packing density with marshalling wiring in process technology, thanks to the modular concept and the compact design.

freistellen mit Pfad CD-Inlay einbauen Network Interfaces fg

The individual marshalling patchboard elements snap into place easily and securely and can also be coded using eleven different colors. This ensures clearly arranged and fault-free wiring. The precise number of positions and the blocked form design, ideal for various applications, create a stable patchboard construction that is resistant to warping. The 2.3 mm test connections are easily accessible, next to the connection points, enabling convenient testing with standard testing accessories. The pre-assembled marshalling patchboards are available with four or six push-in connections per element in 32, 48 and 80-pos. designs. In terms of mounting type, there is a choice of direct, 19″ rack and DIN rail mounting.

The PTRV marshalling terminal system is the most compact on the market with a length of just 100 mm. It offers additions options for easy and clearly arranged marshalling wiring. Its key features include freely selectable colors, easily accessible test connections, and large-surface matrix marking.

The marshalling terminals and marshalling patchboards are designed for use in Ex i safety circuits up to 60 V and are available as blue versions.

The marshalling patchboards, which can be self-assembled, are configured and ordered with just a click of the mouse in the product area on the phoenixcontact.net/products website.