Author Archives: Serene Tan

Serene Tan

About Serene Tan

Serene Tan is the Marketing Communications Executive for Phoenix Contact South East Asia. She is also the editor of the Phoenix Contact Blog.

Four solutions for the PV market

From |

Four solutions from Phoenix Contact that can help you gain competitive advantage in the photovoltaic market

Solar-Farm

1. String Combiner Boxes (SCBs)

In various regions with diverse climatic conditions, achieving maximum availability and performance for a photovoltaic system presents a major challenge for planners and installers.

The important factors here are collecting and distributing string currents, protecting the individual modules againstString combiner boxes damage from lightning and surge voltages, and also monitoring the performance of the system.

Thanks to the use of optimally coordinated components and communication interfaces, the string combiner boxes can be connected to a higher-level park management system quickly and easily.

Phoenix Contact String Combiner Boxes, from 2 to 32 ways, offer:

  • Optimum performance
  • Fast installation and start up
  • Operator satisfaction due to high availability
  • Due and proper consideration of the ambient conditions
  • Optimum positioning of surge protection
  • Use of the best connection technologies and high quality components
  • New compact SCB ( string fusing is done externally with new encapsulated string fuses – this keeps the SCB cool and reduces its size considerably!).

2. Weather Stations

A solution for the evaluation of meteorological sensors for monitoring ambient conditions in weather stationsutility-scale solar power plants.

Fully engineered, boxed solution based on an ILC 171 2TX featuring:

  • all necessary I/O channels
  • surge protection for data and power lines
  • supply option for sensors
  • sensor heating option
  • Ethernet connectivity
  • Standardised MODBUS-Data mapping according to SUNSPEC
  • Simple parametrisation via WEB based management for adjusting sensor types and signal ranges

3. Array controllers

Each fully engineered, boxed solution is controlled by a PLC. PLC programming for all arrays can be identical.   Tasks on array level:Array controllers

  • Aquisition and preprocessing of all relevant data for monitoring (string monitoring, local ambient parameters, inverter data …)
  • Retransmission of monitored data to master PLC/IPC/SCADA in the central control room via a standardized data model (e.g. SUNSPEC/IEC 60870 …)
  • Evaluation of power control commands from master PLC and corresponding control of the inverters with respect to effective and reactive power.

Individual arrays are networked to central control room via appropriate  network infrastructure, e.g. fiber-optic ethernet/MODBUS TCP

4. SolarWorx solar library

The Application:

In recent years, the programming standard IEC 61131 has become established in automation Solarworxtechnology. This standardisation provides many advantages that can also be used for the solar industry. The Solarworx function block libraries are optimally tailored to our Inline and Axioline automation systems. For the user, this means less complex and more functions during planning and implementing solar projects. Training times and therefore costs can be kept low and system documentation becomes more transparent.

In order to keep risks during project planning and implementation as low as possible, EPCs require flexible and scalable concepts for photovoltaic systems as well as calculable software engineering options.

Customer requirements:

System integrators, however, set value on the compatibility of the individual park devices, such as string combiner boxes, inverters, energy meters and power managers. Often, system integrators are lacking the staff and know-how that they would need to implement programming for the automation of a solar park themselves. Setup and start up must be implemented quickly to enable prompt supply of the network with the generated current. Companies charged with the operation and maintenance of photovoltaic systems usually depend on fast error detection and troubleshooting.

The Solution:

The Solarworx function block libraries were created to make the creation and startup of photovoltaic projects with automation components easier and faster. This facilitates the planning and implementation of photovoltaic projects. The customer does not need to have in-depth programming knowledge as the pre-programmed blocks must only be connected with one another. Solarworx offers three different function block libraries for different tasks during the implementation of photovoltaic projects. The following figure gives an overview of the Solarworx structure. So far, there are three function block libraries: Solar Basic, Solar Advanced and Solar Add On.

Phoenix are currently working on additional function block libraries, which will be released soon.

 

*Editor’s Note: This post was originally published in Phoenix Contact Untied Kingdom’s Blog

Ursula Lampmann, partner of Phoenix Contact, has passed away

From |

Lampmann, Ursula

Ursula Lampmann, partner of Phoenix Contact, died on Friday, 26 June 2015, at the age of 94 years in Blomberg. Born in Essen, she joined the company in 1937 and headed the commercial areas as partner of Phoenix Contact for more than five decades. Above all, with her far-sighted handling of the finances she played a crucial role in the successful growth of the company, from small beginnings to global player in the industry.

With her kind and open-minded personality and her appreciative manner she shaped the corporate culture and spirit of Phoenix Contact. She retired in 1995. As requested by the deceased, the funeral took place in the narrowest family circle.

Happy Mother’s Day To All Mothers

From |

“Mothers hold their children’s hands for a short while, but their hearts forever ” – Anonymous

Phoenix Contact wishes Happy Mother’s Day to all mothers out there!

MothersDay2015-D1-blog

 

Phoenix Contact expects revenues of eight percent for 2015, a sign of excellent growth

From |

Bent_Stührenberg_PK2015

Chief Executive Officer Frank Stührenberg expressed his “delight at the results for 2014” during a press conference on Phoenix Contact’s economic growth for the past year. The corporate group’s revenues grew by 8.5 percent to €1.775 billion. “We have tripled our revenues within 15 years,” says Stührenberg, highlighting the successful results. The industrial electronics manufacturer invested €125 million in the expansion of the corporate group. An 11,000-m² innovation and production center was opened in the U.S., where 250 employees work in research and development, marketing, and production. The global workforce increased by approximately 1,100 new employees.

Phoenix Contact is expecting revenue growth of eight percent for the current year. Stührenberg is optimistic in his outlook. “We are seeing a growth in the markets where Phoenix Contact already has a strong presence and our products have already been in use for a long time.” These include the market segments of infrastructure, energy distribution, and renewable energy. The company wants to invest approximately €150 million in national and international expansion activities. A new building in Bad Pyrmont, Germany, will provide an office and lab space of 18,000 m² for the corporate group’s ability to provide expert solutions. Completion is slated for the end of 2016. Phoenix Contact E-Mobility GmbH will establish a subsidiary in China, the world’s largest electromobility market, in the third quarter of 2015. An investment of €20 million will increase production volumes at the site in Nowy Tomy?l, Poland. On 1 September, 100 trainees will embark on a new career, and almost half of them will start in July already as part of their dual education study program.

Touted as the economic barometer of consumer confidence, the Hanover Trade Show begins on 13 April. India is the partner country this year. The electronics specialist will present its innovations and forward-looking technologies at the 2,300-m² exhibition space. One of the main topics will be Industry 4.0, a guiding principle that demonstrates how digitalization is changing not only society but industrial processes, as well. Visitors can experience the continuous data flow live in Hall 8. Here the companies Eplan, Rittal, and Phoenix Contact will be demonstrating a continuous, automated process, from the digitization of an item to its engineering and production. “The Hanover Trade Show has traditionally been a key international trade show for us,” explains Stührenberg. “This year, we will be exhibiting more than 100 innovations and are expecting delegations from more than 50 countries with over 1,000 visitors.”

New Phoenix Contact catalogue app can be downloaded in App Store

From |

Our new version of our Phoenix Contact catalogue app can be downloaded in App Store. Initially, the new version is offered in English and German for iOS devices. A version for Android devices and additional languages are being prepared for the course of 2015.

Find information quickly with the new catalog app

With the new catalog app, you can access our complete product range by navigating through the familiar Phoenix Contact product structure. Intuitive navigation and different check lists will make it a lot easier for you to place your order. Always find the right contact person, and the information fitting your needs.

New functions:

Our product portfolio at a glance:

You can easily navigate through our product range with the new catalog app. Exportable checklists make it easier for you to place your order.

Your advantages

• Navigating, browsing, searching: there are many ways to find the product you need

• Find information quickly in the familiar Phoenix Contact product structure

• Knowing what‘s new: we‘ll keep you informed about new products

• Fast, easy, and modern: accessing information via QR codes

• Up to date: receive the latest information from the Phoenix Contact world

• Exportable check lists: save time when placing your order

Download it now!

PxC App phoneQR Code for App

Happy Easter Day!

From |

Easter2015-D4-v2

Do you know…

Easter is understood to include Good Friday and Easter Sunday, which are three days apart. However Easter truly refers to Easter Sunday – the day on which the resurrection of Jesus is remembered and celebrated.

Easter is the most ancient of Christian festivals, it is older than Christmas, and is considered the most important date in the Christian calendar.

Happy Easter Day! Cheers

Introducing 2 New Products of Phoenix Contact

From |

Powerful New Safety Relays are Just 6mm Wide

The new PSR Mini relays from Phoenix Contact are the world’s slimmest safety relays with the power of a large safety relay. With their compact 6-mm width, they ensure high safety thanks to positively driven contacts.

Phoenix Contact’s new relay technology makes this compact design possible. The design is based on a slim but powerful basic relay characterized by minimal space requirements, low energy consumption, and high system availability.

The safety relays switch loads up to 6 amperes, are compatible with many signal transducers, and can be used in many different applications thanks to extensive approvals. This makes the new products especially suitable for mechanical engineering and process industry applications.

4706

For users, these slim modules require up to 70 percent less space. Since only a single enabling contact is needed, applications can be built with new and improved cost-effectiveness. Safety relays can even be used to build distributed systems in potentially explosive areas. The terminal carriers also enable the use of system cabling solutions for a fast and correct start-up and field connection.

The complete PSR Mini range of safety relays consists of 6-mm and 12-mm models.

 

New EH Housing from Phoenix Contact

Introducing the latest addition to housing family, EH housing – the universal housing system with modular concept which is tailored for your electronic application needs.

EH housing offers you simple design-in, thanks to its variable housing form factor – high and flat design!

Pic 1                        Pic 2

Let us look into details of this marvelous housing family. For a functional device concept, PCBs can be installed in all three space direction. Free choices of PCB connection technologies are available from Phoenix Contact. We have them all incorporated seamlessly into our latest EH housing. From conventional terminal blocks, plug and headers, to RJ 45, or even USB ports, to cover your wide range of today’s electronic application!

Pic 3

Pic 4

Do you want to house your PCB?

Do you want to save more to maximize your profit for your product?

Do you want your PCB to be covered within Phoenix Contact superb quality and reliable housing?

Talk to us now! We are always available for you!