Tag Archives: heavy duty connectors

Heavycon coding options

From |

Written by Scott Mulholland, Product Manager- Industrial Components

I’ve had a number of queries recently regarding coding for our Heavycon range of heavy duty connectors. Coding can become a good idea when your application has a number of similar, or identical, connectors in close proximity like the ones on the side of this panel in this image:

Continue reading

Heavy Duty Connector Configurator

From |

Written by Scott Mulholland, Product Manager- Industrial Components

Good morning everyone. If you’re reading this, you survived the weekend. Perhaps like me, you watched incredulously as your neighbour excitedly covered the whole frontage of their house in Christmas paraphernalia in the first half of November. Be vigilant, these people walk among us.

Anyway, back to reality.

A significant amount of effort goes into maintaining and developing our website to help you find the right products for your applications. It’s one of our best kept secrets that we have a suite of product configurators that all reside in the same place on our website.

If you go to the Phoenix Contact UK homepage and select the ‘Products’ drop down button, you will be presented with the image below. On the right of the screen you will also see ‘ADDITIONAL RESOURCES’ and below that ‘Configurators’. This is where they all live.

Continue reading

The Future is Electric

From |

Written by Duncan Nicol

For thousands of years we have relied on carbon fuels to power our world and for a long time, it made a lot of sense. Carbon fuels such as coal and oil were easy to get to and therefore a cheap source of fuel and energy dense. As demand increased they became harder to find and then, of course, the environmental impact became widely known, but by then we were so very dependent on them. Continue reading

Happy New Year – Let’s take a look at what is in store for 2018…

From |

Welcome to a brand new year of blogging.  As always, our marketing department has a busy year of exhibitions and seminars planned.  Why not join us at one of our events?  Meet our industry specialists and discover more about new products that will be launched this year.After an incredibly exciting 2017, we are raring to go into 2018 and here’s what we have in store for you this year. We have waved goodbye to 2017 and 2018 is going to be an event filled year!

Continue reading

Heavycon heavy-duty connector configurator with 3D visualisation

From |

Written by Scott Mulholland, Product Manager- Industrial Components

Heavycon connectorsAnyone who has ever tried to configure a heavy duty connector from the main components (hood, base, inserts, glands etc) will know that the number of components to choose from is huge. The upside of having this large number of components from which to select the ideal connector solution for your application can sometimes have the downside of perhaps having too much to choose from.

Continue reading

Heavycon Modular- endless possibilities!

From |

Written by Scott Mulholland, Product Manager- Industrial Components

The Phoenix Contact Heavycon range of heavy duty connectors already has a vast array of housings/hoods, bases and inserts offering unparalleled levels of configuration and choice. We also know that every eventuality/configuration cannot be provided, but with the newly enhanced modular connector offer, we go the extra mile in providing you with the modular inserts that you can tailor to your specific needs.

Our innovative ‘snap-in one piece frame’ makes the completion of your connector build that much easier and faster. The snap-in frame fits in all housings from the HEAVYCON STANDARD, EVO, and ADVANCE series. Modules and frames are compatible with the DIN market standard. An added benefit of our frame is that you can actually remove and insert modules whilst they are in the connector base and can even be moved/replaced whilst in the panel!

Continue reading

Heavycon Evo Series- Where less most definitely equals more

From |

Written by Scott Mulholland, Product Manager-  Industrial Components

At Phoenix Contact we understand the problems that Machine Builders will come up against at concept, design, prototyping, testing and field testing. That’s why we put the features and benefits into our products to help you achieve your machine goals.

Our Heavycon Evo series (Part of the Phoenix Contact Heavycon Complete heavy duty offer) has been developed with the Machine Builder firmly in mind. Continue reading

Heavycon Evo plastic range update

From |

Written by Scott Mulholland, Product Manager- Industrial Components

Heavycon Evo Combinations

Within one size sleeve housing, 8 variants can be achieved.

The Heavycon Evo B series plastic range, manufactured in fiberglass-reinforced Polyamide was first launched in 2013. The product offered many features and benefits. Being able to combine cable glands in both vertical and horizontal orientation on the same sleeve housing allowed users to reduce the number of different housings required by 70% compared to industry standard aluminum housings.

The matching cable glands for clamp sizes M20 to M40 could be freely combined with any sleeve and base element in sizes B6, B10, B16, and B24, minimising the number of variants. This reduced stock holding overheads and reduced time spent on design by using components that were quick and easy to assemble contributing to overall savings.

Continue reading