{"id":3740,"date":"2026-04-20T10:09:55","date_gmt":"2026-04-20T06:09:55","guid":{"rendered":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/?p=3740"},"modified":"2026-04-27T10:48:04","modified_gmt":"2026-04-27T06:48:04","slug":"interface-solutions-for-explosion-protection","status":"publish","type":"post","link":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/","title":{"rendered":"Interface solutions for explosion protection"},"content":{"rendered":"\n<h2 class=\"wp-block-heading\"><strong>Compatible, efficient, and usable worldwide<\/strong><\/h2>\n\n\n\n<p class=\"wp-block-paragraph\"><a href=\"https:\/\/www.phoenixcontact.com\/en-ae\/certifications-and-approvals\/explosion-protection\">Explosion protection<\/a> is becoming increasingly important, especially with the growing relevance of green hydrogen. Phoenix Contact therefore offers state\u2011of\u2011the\u2011art interface solutions for explosion\u2011protected applications.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><a href=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"819\" src=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500-1024x819.jpg\" alt=\"\" class=\"wp-image-3742\" style=\"width:700px;height:auto\" srcset=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500-1024x819.jpg 1024w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500-300x240.jpg 300w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500-768x614.jpg 768w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500-624x499.jpg 624w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg 1500w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/a><\/figure>\n<\/div>\n\n\n<!--more-->\n\n\n\n<p class=\"wp-block-paragraph\">In measurement and control technology, intrinsic safety (Ex i) has become a cost\u2011efficient, low\u2011maintenance protection method. Unlike flameproof enclosures (Ex d), it is more economical and allows maintenance and modifications during operation. Ex i applies to the entire circuit, limiting energy so that even in a fault condition, no ignition can occur from sparks or heat.<\/p>\n\n\n\n<p class=\"wp-block-paragraph\">An intrinsically safe circuit typically includes:<\/p>\n\n\n\n<ul class=\"wp-block-list\">\n<li>Intrinsically safe equipment installed in the Ex area (Ex i field device)<\/li>\n\n\n\n<li>Associated equipment located in the non\u2011Ex area (Ex i isolator)<\/li>\n\n\n\n<li>Connecting cables<\/li>\n<\/ul>\n\n\n\n<p class=\"wp-block-paragraph\">Ex i isolators are crucial: they electrically separate the Ex i circuit from the non\u2011Ex i circuit per IEC\/EN 60079\u201111, preventing faults from transferring, and they limit the energy entering the Ex area to a non\u2011ignitable level.<\/p>\n\n\n\n<p class=\"wp-block-paragraph\">Modern Ex i versions of the Mini Analog Pro and Macx Analog families offer broad compatibility with Ex i field devices and support long cable runs. Their Ex i signal conditioners are ATEX\u2011approved for use up to Ex zone 0 (gas) and zone 20 (dust), across all zones and substance groups\u2014including IIC for hydrogen. All devices, including non\u2011Ex i versions, can also be installed in Ex zone 2 under Ex ec, supporting decentralized automation. Additional approvals such as IECEx, UL, CCC, and INMETRO enable global use.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Customized Ex\u00a0i solutions for all applications<\/strong><\/h2>\n\n\n\n<p class=\"wp-block-paragraph\">Phoenix Contact\u2019s Ex i signal conditioners and measuring transducers include customized interface solutions, from individually wired DIN\u2011rail devices for small to medium signal volumes to system\u2011wiring solutions for large volumes. They also support plug\u2011and\u2011play connectivity for standard and universal I\/O cards.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Compact Mini\u00a0Analog\u00a0Pro product family<\/strong><\/h2>\n\n\n\n<p class=\"wp-block-paragraph\">The compact Mini Analog Pro Ex i signal conditioners and measuring transducers combine intrinsic safety and SIL 3 (1oo1) functional safety in just 6.2 mm, saving up to 50% space compared to standard devices while covering key functions (AI, AO, DI, DO, temperature). Non\u2011Ex i versions also offer limit switching, frequency measurement, and signal doubling. They operate from -40\u00b0C to 70\u00b0C and feature a user\u2011friendly design, flexible configuration, digitalization options, and optional communication gateways. Pluggable coded terminal blocks simplify replacement and prevent wiring errors, while the service position safely separates signal and supply circuits for commissioning and maintenance. Integrated test points allow current measurement during operation without interrupting the loop.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Macx\u00a0Analog series with a wide range of functions<\/strong><\/h2>\n\n\n\n<p class=\"wp-block-paragraph\">The Macx Analog series of functionally safe Ex i signal conditioners and measuring transducers. Proven internationally since 2008 and continually expanded. It offers a wide range of functions in a 12.5 mm width. The portfolio includes single\u2011 and two\u2011channel modules for all standard functions (AI, AO, DI, DO, temperature), as well as signal duplicators, limit switches, and specialized Ex i relay modules. Higher\u2011function modules from 17.5 to 35 mm complete the range, such as universal temperature transducers with three relay outputs plus an analog output, and versions with a wide\u2011range 24\u2013230 V AC\/DC supply.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Functionally safe design<\/strong><\/h2>\n\n\n\n<div class=\"wp-block-media-text is-stacked-on-mobile\"><figure class=\"wp-block-media-text__media\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"819\" src=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00159483_5x4_1500-1024x819.jpg\" alt=\"\" class=\"wp-image-3743 size-full\" srcset=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00159483_5x4_1500-1024x819.jpg 1024w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00159483_5x4_1500-300x240.jpg 300w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00159483_5x4_1500-768x614.jpg 768w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00159483_5x4_1500-624x499.jpg 624w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00159483_5x4_1500.jpg 1500w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure><div class=\"wp-block-media-text__content\">\n<p class=\"wp-block-paragraph\">The intrinsically safe Mini Analog Pro versions and the entire Macx Analog range are consistently developed to meet IEC\/EN 61508 safety requirements and are regularly updated to comply with the latest standards. They are suitable for safety\u2011related applications up to SIL 2 SC3 and SIL 3. Additionally, Macx Analog includes versions certified to EN ISO 13849 performance levels, completing the portfolio for machine\u2011building applications.<\/p>\n<\/div><\/div>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Combinable via a standardized feed-in concept<\/strong><\/h2>\n\n\n\n<div class=\"wp-block-media-text has-media-on-the-right is-stacked-on-mobile\"><div class=\"wp-block-media-text__content\">\n<p class=\"wp-block-paragraph\">The Mini Analog Pro and Macx Analog families offer high flexibility and efficiency in analog signal conditioning, supported by a modular supply concept. The robust T\u2011bus DIN\u2011rail connector provides seamless power bridging and group error indication. This enables simple, space\u2011saving power distribution to multiple signal conditioners without additional wiring.<\/p>\n<\/div><figure class=\"wp-block-media-text__media\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"819\" src=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00183850_5x4_1500-1024x819.jpg\" alt=\"\" class=\"wp-image-3744 size-full\" srcset=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00183850_5x4_1500-1024x819.jpg 1024w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00183850_5x4_1500-300x240.jpg 300w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00183850_5x4_1500-768x614.jpg 768w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00183850_5x4_1500-624x499.jpg 624w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00183850_5x4_1500.jpg 1500w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure><\/div>\n\n\n\n<p class=\"wp-block-paragraph\">A key advantage is the easy scalability of the supply system: additional T\u2011bus connectors can be added with minimal effort. Both product families are fully compatible, allowing Mini Analog Pro and Macx Analog devices to be combined on the same T\u2011bus using a standardized supply and error\u2011indication concept. A dedicated divider plate ensures safe mixed installations, from classic measurement and control tasks to SIL 3 and Ex i applications. Integration into third\u2011party systems is also possible via the T\u2011Bus PR adapter. This enables Phoenix Contact signal conditioners to fit existing supply infrastructures without costly modifications.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Various configuration options<\/strong><\/h2>\n\n\n\n<div class=\"wp-block-media-text is-stacked-on-mobile\" style=\"grid-template-columns:39% auto\"><figure class=\"wp-block-media-text__media\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"819\" src=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00032319_5x4_1500-1024x819.jpg\" alt=\"\" class=\"wp-image-3745 size-full\" srcset=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00032319_5x4_1500-1024x819.jpg 1024w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00032319_5x4_1500-300x240.jpg 300w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00032319_5x4_1500-768x614.jpg 768w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00032319_5x4_1500-624x499.jpg 624w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00032319_5x4_1500.jpg 1500w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure><div class=\"wp-block-media-text__content\">\n<p class=\"wp-block-paragraph\">Both product families offer multiple configuration options. Processor\u2011based devices can be connected to a PC via a programming adapter and configured without a supply voltage using the free Clipx Engineer software. The software focuses on ease of use, providing wizards for guided configuration and device replacement, along with comprehensive monitoring functions.<\/p>\n<\/div><\/div>\n\n\n\n<p class=\"wp-block-paragraph\">A manufacturer\u2011independent FDT\/DTM configuration option is also available. Both product families additionally offer DIP\u2011switch settings with easily accessible interfaces when installed. Mini Analog Pro devices can also be configured via NFC using the free <a href=\"https:\/\/www.phoenixcontact.com\/en-us\/products\/signal-conditioners-and-measuring-transducers\">Signal Conditioner<\/a> App. While the Macx Analog series provides extra module information and a DIP\u2011switch setting aid.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Digital nameplate and NE\u00a095 type tests<\/strong><\/h2>\n\n\n\n<div class=\"wp-block-media-text has-media-on-the-right is-stacked-on-mobile\" style=\"grid-template-columns:auto 55%\"><div class=\"wp-block-media-text__content\">\n<p class=\"wp-block-paragraph\">In the age of Industry 4.0, fast and universal digital access to information is essential. Device QR codes provide immediate access to all required data in line with IDTA standards. Since these devices have life cycles of over 20 years, updates to approvals or technical properties are inevitable.<\/p>\n<\/div><figure class=\"wp-block-media-text__media\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"819\" src=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00225986_5x4_1500-1024x819.jpg\" alt=\"\" class=\"wp-image-3746 size-full\" srcset=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00225986_5x4_1500-1024x819.jpg 1024w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00225986_5x4_1500-300x240.jpg 300w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00225986_5x4_1500-768x614.jpg 768w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00225986_5x4_1500-624x499.jpg 624w, https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00225986_5x4_1500.jpg 1500w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure><\/div>\n\n\n\n<p class=\"wp-block-paragraph\"> The digital nameplate ensures users always access the correct, revision\u2011specific documents, data sheets, operating instructions, approvals, drawings, declarations, hardware versions, and relevant firmware. This eliminates time\u2011consuming searches and saves time, money, and resources.<\/p>\n\n\n\n<p class=\"wp-block-paragraph\">An independent Namur test laboratory has performed NE 95 type tests on the Macx Analog and Mini Analog Pro families. The reports confirm efficient space use, installation, and maintenance, and full compliance with all tested Namur recommendations and worksheets. This ensures the devices meet the chemical industry\u2019s high requirements and eliminates the need for users to conduct time\u2011consuming factory tests.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Easy connection to system solutions and digital networks<\/strong><\/h2>\n\n\n\n<p class=\"wp-block-paragraph\">With plug\u2011in communication modules, the Mini Analog Pro family enables convenient conversion of field signals into digital protocols without requiring extra space. The modules support Profinet, Modbus\/TCP, Modbus\/RTU, and Profibus. Up to eight freely combinable signal conditioners form the basis for the gateways, which start up immediately and need no external power supply. Direct signal connection to digital networks, combined with channel\u2011specific isolation and precise transmission, eliminates the need for an I\/O layer and costly special input cards, enabling new, space\u2011saving applications, including for Ex i signals.<\/p>\n\n\n\n<p class=\"wp-block-paragraph\">In large process engineering systems, thousands of signals often need processing, and individually wired DIN\u2011rail devices require extensive installation effort. The Termination Carrier provides a compact alternative, enabling fast, error\u2011free plug\u2011and\u2011play connection to I\/O cards from various manufacturers using pre\u2011assembled system cables. Built on a robust aluminum profile, it accommodates 8 to 32 Mini Analog Pro or Macx Analog signal conditioners and includes a mechanically decoupled marshalling board with a system plug. Its space\u2011saving, durable design, accessible connections, and easy rail mounting simplify installation and servicing while improving system availability. Users also benefit from needing only one signal\u2011conditioner housing design for both individual and system applications.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Saving on marshalling and interface cabinets<\/strong><\/h2>\n\n\n\n<p class=\"wp-block-paragraph\">VIP I\/O marshalling provides an interface system for universal I\/O cards. With a universal 16\u2011channel base module, plug\u2011in function modules, and system cables, it combines signal marshalling and processing in one system. Field signals connect directly to the base element, and functions are adapted by inserting the required modules. This removes the need for marshalling and interface cabinets, eliminates cross\u2011wiring, and shortens project processing times.<\/p>\n\n\n\n<p class=\"wp-block-paragraph\">Learn more about <a href=\"https:\/\/www.phoenixcontact.com\/en-us\/products\/signal-conditioners-and-measuring-transducers\">Signal conditioners and measuring transducers<\/a>.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Compatible, efficient, and usable worldwide Explosion protection is becoming increasingly important, especially with the growing relevance of green hydrogen. Phoenix Contact therefore offers state\u2011of\u2011the\u2011art interface solutions for explosion\u2011protected applications.<\/p>\n","protected":false},"author":357,"featured_media":0,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"footnotes":""},"categories":[1],"tags":[],"class_list":["post-3740","post","type-post","status-publish","format-standard","hentry","category-uncategorized"],"yoast_head":"<!-- This site is optimized with the Yoast SEO plugin v24.7 - https:\/\/yoast.com\/wordpress\/plugins\/seo\/ -->\n<title>Interface solutions for explosion protection | Middle East<\/title>\n<meta name=\"description\" content=\"Explosion protection products from Phoenix Contact for the highest level of safety in potentially explosive areas.\" \/>\n<meta name=\"robots\" content=\"index, follow, max-snippet:-1, max-image-preview:large, max-video-preview:-1\" \/>\n<link rel=\"canonical\" href=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/\" \/>\n<meta property=\"og:locale\" content=\"en_US\" \/>\n<meta property=\"og:type\" content=\"article\" \/>\n<meta property=\"og:title\" content=\"Interface solutions for explosion protection | Middle East\" \/>\n<meta property=\"og:description\" content=\"Explosion protection products from Phoenix Contact for the highest level of safety in potentially explosive areas.\" \/>\n<meta property=\"og:url\" content=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/\" \/>\n<meta property=\"og:site_name\" content=\"Middle East\" \/>\n<meta property=\"article:published_time\" content=\"2026-04-20T06:09:55+00:00\" \/>\n<meta property=\"article:modified_time\" content=\"2026-04-27T06:48:04+00:00\" \/>\n<meta property=\"og:image\" content=\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg\" \/>\n\t<meta property=\"og:image:width\" content=\"1500\" \/>\n\t<meta property=\"og:image:height\" content=\"1200\" \/>\n\t<meta property=\"og:image:type\" content=\"image\/jpeg\" \/>\n<meta name=\"author\" content=\"Rehab Saleh\" \/>\n<meta name=\"twitter:card\" content=\"summary_large_image\" \/>\n<meta name=\"twitter:label1\" content=\"Written by\" \/>\n\t<meta name=\"twitter:data1\" content=\"Rehab Saleh\" \/>\n\t<meta name=\"twitter:label2\" content=\"Est. reading time\" \/>\n\t<meta name=\"twitter:data2\" content=\"7 minutes\" \/>\n<script type=\"application\/ld+json\" class=\"yoast-schema-graph\">{\"@context\":\"https:\/\/schema.org\",\"@graph\":[{\"@type\":\"WebPage\",\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/\",\"url\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/\",\"name\":\"Interface solutions for explosion protection | Middle East\",\"isPartOf\":{\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#website\"},\"primaryImageOfPage\":{\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#primaryimage\"},\"image\":{\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#primaryimage\"},\"thumbnailUrl\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500-1024x819.jpg\",\"datePublished\":\"2026-04-20T06:09:55+00:00\",\"dateModified\":\"2026-04-27T06:48:04+00:00\",\"author\":{\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#\/schema\/person\/f082d19c085d32a2ba4d429127104281\"},\"description\":\"Explosion protection products from Phoenix Contact for the highest level of safety in potentially explosive areas.\",\"breadcrumb\":{\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#breadcrumb\"},\"inLanguage\":\"en-US\",\"potentialAction\":[{\"@type\":\"ReadAction\",\"target\":[\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/\"]}]},{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#primaryimage\",\"url\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg\",\"contentUrl\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg\",\"width\":1500,\"height\":1200},{\"@type\":\"BreadcrumbList\",\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#breadcrumb\",\"itemListElement\":[{\"@type\":\"ListItem\",\"position\":1,\"name\":\"Home\",\"item\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/\"},{\"@type\":\"ListItem\",\"position\":2,\"name\":\"Interface solutions for explosion protection\"}]},{\"@type\":\"WebSite\",\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#website\",\"url\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/\",\"name\":\"Middle East\",\"description\":\"PHOENIX CONTACT\",\"potentialAction\":[{\"@type\":\"SearchAction\",\"target\":{\"@type\":\"EntryPoint\",\"urlTemplate\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/?s={search_term_string}\"},\"query-input\":{\"@type\":\"PropertyValueSpecification\",\"valueRequired\":true,\"valueName\":\"search_term_string\"}}],\"inLanguage\":\"en-US\"},{\"@type\":\"Person\",\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#\/schema\/person\/f082d19c085d32a2ba4d429127104281\",\"name\":\"Rehab Saleh\",\"image\":{\"@type\":\"ImageObject\",\"inLanguage\":\"en-US\",\"@id\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#\/schema\/person\/image\/\",\"url\":\"https:\/\/secure.gravatar.com\/avatar\/50c529c9e01c93ce87ad2a7073c25b0fe60586e0be6673ecb4fafb48b3acc8ca?s=96&d=mm&r=g\",\"contentUrl\":\"https:\/\/secure.gravatar.com\/avatar\/50c529c9e01c93ce87ad2a7073c25b0fe60586e0be6673ecb4fafb48b3acc8ca?s=96&d=mm&r=g\",\"caption\":\"Rehab Saleh\"},\"url\":\"https:\/\/blog.phoenixcontact.com\/marketing-ae\/author\/vml9bt\/\"}]}<\/script>\n<!-- \/ Yoast SEO plugin. -->","yoast_head_json":{"title":"Interface solutions for explosion protection | Middle East","description":"Explosion protection products from Phoenix Contact for the highest level of safety in potentially explosive areas.","robots":{"index":"index","follow":"follow","max-snippet":"max-snippet:-1","max-image-preview":"max-image-preview:large","max-video-preview":"max-video-preview:-1"},"canonical":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/","og_locale":"en_US","og_type":"article","og_title":"Interface solutions for explosion protection | Middle East","og_description":"Explosion protection products from Phoenix Contact for the highest level of safety in potentially explosive areas.","og_url":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/","og_site_name":"Middle East","article_published_time":"2026-04-20T06:09:55+00:00","article_modified_time":"2026-04-27T06:48:04+00:00","og_image":[{"width":1500,"height":1200,"url":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg","type":"image\/jpeg"}],"author":"Rehab Saleh","twitter_card":"summary_large_image","twitter_misc":{"Written by":"Rehab Saleh","Est. reading time":"7 minutes"},"schema":{"@context":"https:\/\/schema.org","@graph":[{"@type":"WebPage","@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/","url":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/","name":"Interface solutions for explosion protection | Middle East","isPartOf":{"@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#website"},"primaryImageOfPage":{"@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#primaryimage"},"image":{"@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#primaryimage"},"thumbnailUrl":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500-1024x819.jpg","datePublished":"2026-04-20T06:09:55+00:00","dateModified":"2026-04-27T06:48:04+00:00","author":{"@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#\/schema\/person\/f082d19c085d32a2ba4d429127104281"},"description":"Explosion protection products from Phoenix Contact for the highest level of safety in potentially explosive areas.","breadcrumb":{"@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#breadcrumb"},"inLanguage":"en-US","potentialAction":[{"@type":"ReadAction","target":["https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/"]}]},{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#primaryimage","url":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg","contentUrl":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-content\/uploads\/sites\/9\/2026\/04\/00224376_5x4_1500.jpg","width":1500,"height":1200},{"@type":"BreadcrumbList","@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/interface-solutions-for-explosion-protection\/#breadcrumb","itemListElement":[{"@type":"ListItem","position":1,"name":"Home","item":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/"},{"@type":"ListItem","position":2,"name":"Interface solutions for explosion protection"}]},{"@type":"WebSite","@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#website","url":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/","name":"Middle East","description":"PHOENIX CONTACT","potentialAction":[{"@type":"SearchAction","target":{"@type":"EntryPoint","urlTemplate":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/?s={search_term_string}"},"query-input":{"@type":"PropertyValueSpecification","valueRequired":true,"valueName":"search_term_string"}}],"inLanguage":"en-US"},{"@type":"Person","@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#\/schema\/person\/f082d19c085d32a2ba4d429127104281","name":"Rehab Saleh","image":{"@type":"ImageObject","inLanguage":"en-US","@id":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/#\/schema\/person\/image\/","url":"https:\/\/secure.gravatar.com\/avatar\/50c529c9e01c93ce87ad2a7073c25b0fe60586e0be6673ecb4fafb48b3acc8ca?s=96&d=mm&r=g","contentUrl":"https:\/\/secure.gravatar.com\/avatar\/50c529c9e01c93ce87ad2a7073c25b0fe60586e0be6673ecb4fafb48b3acc8ca?s=96&d=mm&r=g","caption":"Rehab Saleh"},"url":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/author\/vml9bt\/"}]}},"_links":{"self":[{"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/posts\/3740","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/users\/357"}],"replies":[{"embeddable":true,"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/comments?post=3740"}],"version-history":[{"count":1,"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/posts\/3740\/revisions"}],"predecessor-version":[{"id":3747,"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/posts\/3740\/revisions\/3747"}],"wp:attachment":[{"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/media?parent=3740"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/categories?post=3740"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blog.phoenixcontact.com\/marketing-ae\/wp-json\/wp\/v2\/tags?post=3740"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}