What challenges does the machine building and systems manufacturing industry face, and how can innovative connectors help address them? Simple, standardized connection processes that can be automated as much as possible are becoming a key driver of efficiency and system availability.
The machine building and systems manufacturing industry is facing profound challenges that are placing increasing pressure on established production processes. In many industrialized nations, experienced professionals are retiring from the workforce, while there is a shortage of qualified young talent. Technical professions that involve hands-on work and experience, such as mechanical engineering, systems manufacturing, and control cabinet building, are being hit especially hard.
Companies must therefore carry out complex electrical engineering tasks with fewer staff. The demands for flexibility, modularity, and cost-effectiveness are increasing, while times-to-market for new machines and systems are shrinking. Industrial companies expect customized solutions, short lead times, and rapid commissioning.
Cabling as a Critical Time and Cost Factor
Against this backdrop, cabling requirements are increasingly becoming a focus of strategic considerations. As a result, companies are reviewing traditional connection concepts more closely. Traditional heavy-duty industrial connectors perform their basic function reliably, but they are often not designed to meet today’s requirements for efficiency, modularity, and compactness.
Traditional heavy-duty connectors are often optimized for a single transmission method, such as power, signals, or data. If multiple types of media must be transmitted, several separate connectors may be required. This affects installation effort, installation space, and costs. Each additional interface means more components, extra wiring, and longer testing and commissioning times. System complexity also increases, reducing clarity, ease of maintenance, and reliability.
The figure on the left illustrates the key features of the click-in technology, including tool-free mounting, media integration, and simplified conductor connection.
A significant portion of installation time is spent assembling and wiring connectors. With a shortage of skilled workers and tight deadlines, these steps become a bottleneck.
Simplification and Process Optimization
Companies are turning to solutions that simplify and accelerate installation and commissioning. These solutions should break down dependencies in existing assembly chains and enable more flexible process design. Clearly defined and reproducible assembly steps can also be carried out partially or fully automatically in the future.
Role of Modern Heavy-Duty Industrial Connectors
Heavy-duty industrial connectors play a key role in this process. The combination of robust housing technology, innovative contact inserts, and modular systems contributes to increasing efficiency. These modular connectors are key components for the All Electric Society.
Phoenix Contact’s new contact inserts and module carrier frames with click-in locking mechanisms enable completely tool-free mounting, from wiring to mechanical fastening inside the housing. The contact inserts are pressed into the housing and snap into place with an audible and tactile click. Integrated locking elements ensure a secure, reliable, and vibration-resistant fit without screws or additional mounting material.
Combined with proven Push-in connection technology, this creates a fully tool-free connection concept. Conductors can be contacted easily and securely. The protective conductor no longer needs to be connected before the contact insert is mounted. Housings can first be assembled mechanically and then wired in a single combined step.
Power, Signal, and Data in One Connector
The click-in module carrier frames provide a refined solution for applications requiring multiple transmission media in one connector. Users select the required power, signal, and data modules, insert them into the frame without tools, and press the frame into the housing. The click-in mechanism immediately locks it securely into place.
Cabling as a Strategic Success Factor
Heavy-duty industrial connectors with click-in locking mechanisms reduce assembly times, eliminate tool-dependent steps, and improve installation reliability. Companies benefit from shorter turnaround times, greater flexibility, and a lasting reduction in the workload of skilled workers while maintaining high quality and reliability.
As complexity and modularity increase and project timelines become shorter, cabling is becoming a strategic factor for success. Such solutions support industry competitiveness and future viability.
Ready to simplify installation and commissioning processes? Discover how Phoenix Contact’s heavy-duty industrial connectors with click-in locking mechanisms enable completely tool-free mounting, reduce assembly times, and support flexible system designs. Learn more about HEAVYCON click-in connection solutions and find the right configuration for your application.